Skip to main content
shinnlin
Associate III
Dec 1, 2004 2:59 AM UTC
Question

Method to disable Write Protection

Posted on December 01, 2004 at 03:59

Method to disable Write Protection

This topic has been closed for replies.

3 replies

shinnlin
shinnlinAuthor
Associate III
Nov 30, 2004 5:17 AM UTC
Posted on November 30, 2004 at 06:17

Flash Write Protection can be disabled temporarily or permanently.

Is the following the right way to do that ?

Temporarily:

Just set the WyRx of FNVWPAR to 1.

Permanently:

use FLASH_WritePrConfig() to disable

shinnlin
shinnlinAuthor
Associate III
Nov 30, 2004 9:04 PM UTC
Posted on November 30, 2004 at 22:04

As Reference Manual v4.0 page 64 states :

2.5.0.3 Temporary Unprotection

The Flash module enables to temporary unprotect a protected sector (write protect), or protected resources (debug access protect).

A write protected sector can be temporarily unprotected by executing the set protection

operation and writing 1 in the associated WyPx bits of FLASH_NVWPAR.

smartpocket
Associate III
Dec 1, 2004 2:59 AM UTC
Posted on December 01, 2004 at 03:59

NOTE: temporariliy unprotect is possible only executing from FLASH. . . .

by

smart