Skip to main content
Associate
August 19, 2025
Question

M41T83ZMY6F RTC Reports Half the Actual Time

I am working with the M41T83ZMY6F RTC (internal crystal version) in a project and I’ve encountered an unusual behavior: when I read the time via I²C, the RTC seems to count at exactly half the expected rate. For example, after one real second, the seconds register increments by 0.5 s equivalent (or appears to update only every 2 seconds).

Interestingly, I have observed that on some boards the RTC works correctly, while on others it exhibits this half-speed behavior.

 

What can cause this ?

 

Thanks

This topic has been closed for replies.

3 replies

Mike_ST
ST Technical Moderator
August 20, 2025

Hello,

In that kind of case, it can be a good idea to dump the registers, and compare working vs non-working case.

You can even post the registers values, perhaps someone will have an idea.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
TDK
August 20, 2025

It's probably also a good idea to show your evidence of the issue. What leads you to believe time is slowing down on some chips? Perhaps there is some other explanation.

"If you feel a post has answered your question, please click ""Accept as Solution""."
shanAuthor
Associate
August 20, 2025

After writing the system time to the RTC in Linux, when I read the RTC time from the Linux terminal after a while, I observe that the RTC is behind the system time by exactly half of the elapsed time.

 

Thanks