Skip to main content
Associate
January 19, 2024
Question

M24C02 POR Threshold

What is the lower limit of the POR threshold value for the M24C02-RMN6TPT?
The datasheet states "lower than the minimum VCC", but we need to know the specific value.
With our hardware, the VCC only goes down to 1.0 V, not 0V.  Therefore, I am inquiring to make sure that Device Reset is working reliably.

This topic has been closed for replies.

4 replies

Mike_ST
ST Technical Moderator
January 22, 2024

Hello,

Your device is M24C02-RMN6TPT, so tables 6 and 21 in the datasheet tell that this value is 1.8V:

R = VCC = 1.8 V to 5.5 V

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Tesla DeLorean
Guru
January 22, 2024

Ok, but that's the voltage range for reliable operation. The question here is more about some degree of viability and retention which is likely much lower.

Is there a POR circuit internally that clamps it in reset below 1.8V ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
January 22, 2024
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
yanaAuthor
Associate
January 22, 2024

Hello,

What is the threshold range that its internal POR operates in?

For example (1.8-1.6V) or (1.8V - 1.4V) or .....?