Skip to main content
Associate
May 1, 2025
Solved

M24512-A125

I intended to write a wrapper to access the memory section of the M24512 part. I began with enumeration using the device identification code, but instead of receiving I2C Family as 0xE0, I got 0xFF, I need to understand what went wrong. Additionally, when I write a byte to memory and read it back, it still shows 0xFF, please find trace logs attached, appreciate your quick reply.Read-Byte.pngWrite-Byte.pngWrong-Family-Code.png

This topic has been closed for replies.
pratapBest answer
Associate
May 1, 2025

I realized my mistake, was using 8bit address and data, not 16bit as expected....!!! Please mark it as done, Thanks

But still the Family ID is wrong...!!!

2 replies

pratapAuthorBest answer
Associate
May 1, 2025

I realized my mistake, was using 8bit address and data, not 16bit as expected....!!! Please mark it as done, Thanks

But still the Family ID is wrong...!!!

Peter BENSCH
ST Technical Moderator
May 1, 2025

Welcome @pratap, to the community!

Great that it works at least partially!

However, you have only included a few screenshots of the logic analyser, but have not shown the relevant program parts, schematics or boundary conditions. Without this information, it will be a bit difficult for the community to understand your problem.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.