Skip to main content
HIsma
Visitor II
Aug 13, 2018 5:02 PM UTC
Question

Low-Side Driver L9825

Hi

I'm using L9825 in one of my applications and have couple of questions just to make sure I get it right:

1- I have Vcc=3.3v and Reset line pulled high. Is that ok?

2- my understanding is that NON1 and NON2 can be used to directly drive OUT1 and OUT2 independently of SPI interface; So after setting NON1 and NON2 to digital low/high, do I need to use the NCS line at all? anything else that I should consider?

Thank you.

This topic has been closed for replies.