Skip to main content
RKurd.1
Associate
May 9, 2022
Solved

Looking for a substitute for the following part STTH512(DPAK) to a SOD132 (DO-123) package.

..

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 10, 2022

So the question is not about an alternative in a smaller enclosure, but about general alternatives due to the current worldwide shortage of components: unfortunately, there is no alternative in the same or compatible package in this power class, only the STTH812 could come into question, but it is only available in larger packages like the thru-hole TO-220AC or the D2PAK. Of course, there are also other devices with an even higher current capability and therefore a much larger package.

Good luck!

If the problem is resolved or answered, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

Peter BENSCH
ST Technical Moderator
May 10, 2022

Welcome, @RKurd.1​, to the community!

The STTH512 is not Discontinued, but Active, which is why I moved it to the Analogue and Audio and Power Management channels.

Regarding your question: the performance (current, power dissipation) of an STTH512B-TR cannot be achieved in the package SOD132 aka SMB, because it is much too small for that. This is already apparent from the dimensions, but also from the thermal resistance. Please multiply the maximum voltage drop with the maximum current and the thermal resistance, then you will see the resulting temperature increase that SMB can no longer handle.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RKurd.1
RKurd.1Author
Associate
May 10, 2022

Yes,

The STTH512B-TR seems to be a popular part and is hard to source. Is there another drop in replacement that is similar or better?

Regards

Ron

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 10, 2022

So the question is not about an alternative in a smaller enclosure, but about general alternatives due to the current worldwide shortage of components: unfortunately, there is no alternative in the same or compatible package in this power class, only the STTH812 could come into question, but it is only available in larger packages like the thru-hole TO-220AC or the D2PAK. Of course, there are also other devices with an even higher current capability and therefore a much larger package.

Good luck!

If the problem is resolved or answered, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.