Skip to main content
David.Cheng
Associate III
October 17, 2019
Question

long press problem

void main(void)
{
 /* Infinite loop */
 
 CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_8);
 
 GPIO_Init(GPIOE, GPIO_Pin_7, GPIO_Mode_In_PU_IT);
 EXTI_setup();
 
 halt(); // first active
 
 
 #if 0
 while(1)
 {
 halt();
 delay_ms(1000);
 
 if(GPIO_ReadInputDataBit(GPIOE, GPIO_Pin_7) == 0)
 {
 //i++;
 //if(i == 25)
 break;
 }
 
 
 }
 #endif
 usart_setup();
 USART_SendData8(USART1, 'a');
 USART_SendData8(USART1, 'b');
 
 while (1)
 {
 }
}
void EXTI_setup(void)
{
 
 ITC_DeInit();
 ITC_SetSoftwarePriority(EXTI7_IRQn, ITC_PriorityLevel_1);
 
 
 EXTI_DeInit();
 
 EXTI_SetPinSensitivity(GPIO_Pin_7, EXTI_Trigger_Falling);
 //EXTI_SetPinSensitivity(GPIO_Pin_7, EXTI_Trigger_Rising);
 //EXTI_SetTLISensitivity(EXTI_TLISENSITIVITY_FALL_ONLY);
 enableInterrupts();
 
}

when in long press, it does not wakeup.

until release , then wakeup

    This topic has been closed for replies.

    4 replies

    JoniS
    Senior
    October 17, 2019

    EXTI_SetPinSensitivity(GPIO_Pin_7, EXTI_Trigger_Rising);

    ​

    Change the trigger for that interrupt to rising edge instead of falling edge, then it should wake up instantly.​

    David.Cheng
    Associate III
    October 17, 2019

    debug long time, falling edge can not

    when change to rising edge , configure pe7 to floating input with it , and gpio connect to gnd directly?

    JoniS
    Senior
    October 17, 2019

    Can you post the schematic how the button is connected?

    ​

    For rising edge to work, the io should be pulled down, and button then connects it to VCC.

    ​

    For falling edge to work, IO should be pulled to VCC, button then grounds it.

    ​

    Based on your initial proplem description i assume the IO is pulled low(gnd) and the button connects to vcc, which would result to behaviour you observe, which is that mcu wakeups when the button is released.​

    David.Cheng
    Associate III
    October 17, 2019

    0690X00000AqTr8QAF.png

    the falling edge one