Skip to main content
hcheng1
Associate
February 2, 2004
Question

Load WinCE to Atlas?

  • February 2, 2004
  • 3 replies
  • 1025 views
Posted on February 02, 2004 at 08:26

Load WinCE to Atlas?

This topic has been closed for replies.

3 replies

hcheng1
hcheng1Author
Associate
August 22, 2003
Posted on August 22, 2003 at 14:01

Did anybody successfully load WinCE.net or early version of WinCE to atlas board? We did it, bit network card driver doesn’t work and the mouse can’t work either. Please give me some guide. Thank you very much!

stephen239955_st
Associate II
December 8, 2003
Posted on December 08, 2003 at 09:39

I have managed to upload an image through the network reliably using an ISA board called Linksys.

It is possible to use PCI based cards and I managed to use a Realtek 8139 but you have to disable to wrtie posting and read prefetch options in the BIOS beforehand.
omuenchow
Associate
February 2, 2004
Posted on February 02, 2004 at 08:26

We use the STPC with Intel 82559ER chip. There are two drivers out there. First one from Intel itself to which works fine on WinCE 4.x and one from FS Force on Platform Builder 3rd Party CD to support Kernel Debugging over Ethernet on Intel chip. Both work fine on our hardware.