Skip to main content
herzog
Visitor II
Mar 6, 2010 1:36 AM UTC
Question

Linux support

Posted on March 06, 2010 at 02:36

What a pity.

If it would support Linux, I could actually use it, now that I have mine - but it seems like Arduino is the way to go.

Another piece of good hardware wasted due to crappy software support...

    This topic has been closed for replies.

    2 replies

    ne562
    Associate III
    Feb 24, 2011 12:47 PM UTC
    Posted on February 24, 2011 at 13:47

    STVD works in Wine, for programming there is only one option - http://www.versaloon.com/bbs/viewtopic.php?f=2&t=17&start=0

    stm2399
    Visitor II
    Mar 9, 2011 8:11 AM UTC
    Posted on March 09, 2011 at 09:11

    The url (thread) andrey points to is for using (converting) the STM8S-Discovery to an ARM SWD debugger. Not to support STM8 SWIM.

    I don't think that will work with the sw/port from that thread.

    The Standard Versaloon dongle should support STM8 SWIM (Simon says)

    /Bingo