Skip to main content
robertpomeroy9
Visitor II
Mar 17, 2010 6:10 PM UTC
Question

Library build project in STVD

Posted on March 17, 2010 at 19:10

Library build project in STVD

    This topic has been closed for replies.

    1 reply

    mozra272
    Visitor II
    May 17, 2011 1:07 PM UTC
    Posted on May 17, 2011 at 15:07

    Hi Robert,

    You need to customizing your linker input settings:

    The input settings interface for the linker allows you to define input sources for the linker such as libraries and vector files, as well as allowing you to define segments in your microcontroller's memory and assign code sections to them. Access this view by selecting

    Input

    in the

    Category

    list box.

    Customizing linker input settingsAuto segment declaration and section assignment

    When the

    Auto

    option is checked the script link file is automatically generated to the output path. The filename by default is

    TargetSName

    .lkf

    . However, by unchecking the

    Auto

    option, you can enter the path and filename that you want for the script link.

    Note: If you have disabled the automatic generation of the script link, it will not be updated if you make changes to your project, such as removing a source file. If you make such a change you will have to edit the script link manually.

    in the last STVD 4.1.4 version the Improvements For Cosmic toolset:

    – Enhancement of lkf file management: sections in the lkf file are reserved for STVD,

    and are updated even if Auto mode is disabled. Automatic management may be

    disabled by removing section delimiters. Custom modifications are allowed in the

    lkf outside reserved sections and when the Auto mode is disabled.

    – Makes symbolic disassembly work for peripheral registers defined in Cosmic

    include files.

    For more details refer to the STVD help and to the STVD 4.1.4 release notes

    Regards

     

    Mozra