Skip to main content
PKoll.1
Visitor II
April 28, 2022
Question

Junction temperature details are not available in M24C64-A125 datasheet. Can someone help me with the data

..

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
April 28, 2022

Welcome, @PKoll.1​, to the community!

The M24C64-A125 has a maximum current consumption of 2mA at 5.5V. We are therefore talking about a maximum power loss of 2mA*5.5V=11mW.

Even if we assume a completely unrealistic value of 100K/W for Rja, this would result in a worst case temperature increase of 1.1K. In this respect, the ambient temperature can be regarded as identical to the junction temperature.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.