Skip to main content
This topic has been closed for replies.

4 replies

davidscaradozzi9
Associate
Jun 8, 2005 11:39 AM UTC
Posted on June 08, 2005 at 13:39

we built a custom board with str711STR711F R2T6. Untill now we use STR7-RVDK + ICE-ME to program the STR710-eval and all goes fine but when we connect to the custom board we receive an error. Is the configuration for the EVAL ok for the str711STR711F R2T6 or we need different device configuration file?

thanks,

David

davidscaradozzi9
Associate
Jun 8, 2005 12:31 PM UTC
Posted on June 08, 2005 at 14:31

> connect,route 1

> connect 5

Advanced_info searched in: Local Advanced_info, CHIP=STR710FZ2, CHIP=STR710FZ2,

CHIP=STR710FZ2

Using Advanced info based on Processor 'ARM'

Using Advanced info based on 'Default' or 'All'

ARM RealView ICE Micro Edition

TurboTAP FPGA Simulator

Copyright ARM Limited 2002,2003

Attached to running device

Mode: Big Endian

Error V000F (Vehicle): Cannot access- connection to target is down

I think the problem is >>> CHIP=STR710FZ2

thanks,

D.

davidscaradozzi9
Associate
Jun 14, 2005 2:20 AM UTC
Posted on June 14, 2005 at 04:20

Sorry, I've checked the pull up of nSTANDBY pin and it's ok.

I try the autoconfig scan chain in the RVConfig tool but without success.

I've upgrade the RVDK to 1.7 version and I obtaign the same results.

Do you know if I need a dedicated configuration file for str711STR711F R2T6 or it's ok the default for STR7-EVAL Board?

davidscaradozzi9
Associate
Jun 15, 2005 9:45 AM UTC
Posted on June 15, 2005 at 11:45

we corrected the nJTRST circuit and we solved the problem.

Thanks,

David