Skip to main content
September 17, 2025
Question

Issues setting up ZY-2.1BT 2.1 Bluetooth amplifier with speakers

Hi everyone,

I recently got a ZY-2.1BT 2.1 channel Bluetooth digital power amplifier board to test out as part of a DIY audio setup. The idea is to run two bookshelf speakers plus a subwoofer from a single board, mainly for a small home theater project.

Setup Details:

  • Power supply: 24V 10A DC adapter

  • Speakers: two 6Ω 50W bookshelf speakers + one 8Ω 80W subwoofer

  • Inputs: tested both Bluetooth (5.1) and AUX from a laptop

  • Connected using the provided DC power plug and screw terminals for speakers

Now here are my issues:

  • At medium to high volumes, I get distortion on the subwoofer even though the speakers sound clean

  • Bluetooth pairing works fine at first, but sometimes audio cuts out randomly for a second or two

  • AUX input works, but there’s a noticeable hum when no music is playing

  • The board gets warm after about 30 minutes of use — not hot enough to shut down, but I’m wondering if I need a heatsink or better airflow

What I’ve tried so far:

  • Swapped in a different subwoofer (4Ω 60W) — distortion still happens at higher volume

  • Tried another power supply (19V 6A) — same results, maybe slightly less hum

  • Moved the board away from other electronics to rule out interference

  • Checked wiring polarity and connections — all look fine

My questions:

  1. Is it normal for the subwoofer channel on the ZY-2.1BT to distort earlier than the stereo channels?

  2. Would running it at 12V vs 24V change the noise floor or stability?

  3. Any tricks for reducing the AUX hum — like grounding the input or shielding cables?

  4. Should I consider adding a small heatsink to this board, or is passive cooling usually enough?

Thanks in advance. I’m hoping to clean up the sound and make this stable for daily use.

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
September 17, 2025

you mean this ?

 

AndrewNeil_1-1758122050321.png

 

 

That's not an ST product - you need to go to the manufacturer and/or supplier for help with it.

https://easyelecmodule.com/contact-us/

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.