Skip to main content
roger_chang
Visitor II
Nov 26, 2010 10:14 AM UTC
Question

Is there Level triger IO interrupt in Str912FAW44

Posted on November 26, 2010 at 11:14

Is there Level triger IO interrupt in Str912FAW44

This topic has been closed for replies.

1 reply

sjackson2
Visitor II
May 17, 2011 8:01 AM UTC
Posted on May 17, 2011 at 10:01

I believe there IS a level triggered IO interrupt available, you just have to configure it through the WIU registers.  There are a number of pins labeled as EXTINT in the datasheet that go to the WIU you can use.  I believe there are 32 available.

Look at the WIU_TR register to set rising/falling edge sensitivity and WIU_MR to set which external interrupt lines you are interested in monitoring.

Hope that helps