Skip to main content
IGent.1
Visitor II
December 13, 2019
Question

Is the MOSFET (STP85NF55L) reliability affected if the Vgs is near to the maximum specified in the datasheet?

My customer specifies a relation of 60% of the maximum Vgs for operation. My design is using 80% of the maximum Vgs. They are asking how this increase will affect the component reliability (failure mechanism, failure rate...).

My design is eqquiped with 4 STP85NF55L, operating at 32Hz (PWM) resistive loads.

This topic has been closed for replies.