Skip to main content
David.Cheng
Associate III
December 2, 2019
Question

is the i2c init function right?

void sEE_Init(void)
{
 
 //printf("i2c init\n");
 sEE_LowLevel_Init(); // enable clock
 
 /*!< I2C configuration */
 /* sEE_I2C Peripheral Enable */
 I2C_Cmd(sEE_I2C, ENABLE);
 I2C_DeInit(sEE_I2C);
 /* sEE_I2C configuration after enabling it */
 I2C_Init(sEE_I2C, I2C_SPEED, I2C_SLAVE_ADDRESS7, I2C_Mode_I2C, I2C_DutyCycle_2,
 I2C_Ack_Enable, I2C_AcknowledgedAddress_7bit);
 
 /* Enable the sEE_I2C peripheral DMA requests */
 //I2C_DMACmd(sEE_I2C, ENABLE);
 
#if defined (sEE_M24C64_32)
 /*!< Select the EEPROM address according to the state of E0, E1, E2 pins */
 sEEAddress = sEE_HW_ADDRESS;
 
#endif /*!< sEE_M24C64_32 */
}

    This topic has been closed for replies.