Skip to main content
mslab
Associate III
Mar 21, 2006 6:06 AM UTC
Question

Is it possible to write into code memory without using IAP ?

Posted on March 21, 2006 at 07:06

Is it possible to write into code memory without using IAP ?

This topic has been closed for replies.

14 replies

laurent239955_stm1
Associate
Mar 14, 2006 4:26 AM UTC
Posted on March 14, 2006 at 05:26

Hi,

Is the same behaviour on the 10 parts ? I mean :

- when you check the failed content, is there several addresses ?

- is(are) the same address(es) from one part to another ?

- is the content changed in the same way ?

By the way, have you a contact in ST sales office or do you get the parts through a distributor.

Best regards

Laurent

mslab
mslabAuthor
Associate III
Mar 14, 2006 4:46 AM UTC
Posted on March 14, 2006 at 05:46

Hi,

- when you check the failed content, is there several addresses ?

YES (E001, E002, E003, E004, ... and sometimes up to the beginning of the code

so the ST7 cannot run!

is(are) the same address(es) from one part to another ?

NO, because some parts

- is the content changed in the same way ?

Often we get 223 (0xDF)

By the way, have you a contact in ST sales office or do you get the parts through a distributor.

In france, through EURODIS (RIP!) and now AVNET

Best regards

B.PICARD

laurent239955_stm1
Associate
Mar 21, 2006 4:12 AM UTC
Posted on March 21, 2006 at 05:12

Hi,

Are they more than 32 bytes which are corrupted ?

Can you try to set the sector 0 size to 4k. This will protect against IAP ?

If you still get the problem, this will come from another source than the IAP.

Best regards

Laurent

mslab
mslabAuthor
Associate III
Mar 21, 2006 6:06 AM UTC
Posted on March 21, 2006 at 07:06

Hi,

Are they more than 32 bytes which are corrupted ?

Sometimes YES and sometimes NO

Our sector 0 size is 0.5 K

Thanks

B.PICARD