Welcome, @PZuko.1, to the community!
Yes, you can do that.
For example, you can connect the STM8 to the PC via ST-LINK and use STVP to make the connection. STVP is included in the software package STVD, which should not be installed in C:\Program Files\ because of irritating spaces (STVD is still from the old Windows era), but as admin in a short path like e.g. C:\ST\STVD
In STVP there are three tabs at the bottom PROGRAM MEMORY, DATA MEMORY and OPTION BYTE, with which you can select the appropriate target area - so for the EEPROM area DATA MEMORY. If you have activated it, you can enter data directly in the EEPROM area, which can be written with
- Program > Current Tab
- Program > Address Range...
With Address Range you define the range to be written, e.g. 1000...100F, which is to be written instead of the entire tab range.
Does it answer your question?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.