Skip to main content
hg-chen
Associate III
Feb 22, 2007 12:29 PM UTC
Question

Is it OK to input periodic pulse for STR711 P0.15/WAKEUP pin?

Posted on February 22, 2007 at 13:29

Is it OK to input periodic pulse for STR711 P0.15/WAKEUP pin?

This topic has been closed for replies.

3 replies

hg-chen
hg-chenAuthor
Associate III
Feb 7, 2007 6:40 AM UTC
Posted on February 07, 2007 at 07:40

the pin P0.15/WAKEUP can be used as input to wake up from standby mode,

it is hign active?

Can a periodic pulse do this function?

kaouther
Associate II
Feb 22, 2007 12:28 PM UTC
Posted on February 22, 2007 at 13:28

Hello,

the P0.15/WAKEUP pin should be at low level to wake up the system from the STANDBY mode. When the WAKEUP pin pin goes high, the MCU will resume from stand by mode. And it is possible to use a periodic pulse for that

;)

kaouther
Associate II
Feb 22, 2007 12:29 PM UTC
Posted on February 22, 2007 at 13:29

Hello,

the P0.15/WAKEUP pin should be at low level to wake up the system from the STANDBY mode. When the WAKEUP pin pin goes high, the MCU will resume from stand by mode. And it is possible to use a periodic pulse for that

;)