Skip to main content
carnett1
Associate III
Nov 12, 2010 1:33 PM UTC
Question

IO ports

Posted on November 12, 2010 at 14:33

I intialize Port A3 as a push pull output but when I call writeHigh or writeLow nothing changes on that output.  I am using a multimeter to read the output on pin 9 of cn1

charles

    This topic has been closed for replies.

    5 replies

    infoinfo967
    Associate II
    Nov 22, 2010 6:19 PM UTC
    Posted on November 22, 2010 at 19:19

    Hi,

    I'm not a crack but Brazov told me in a similar question:

    before putting a data output on portA, you need to configure the port:

    LD A, #255

    LD $5002, A ;output push pull 

    LD $5003, A ; see page 101

    brazov2

    In your case , you need:

    LD A, #255

    LD $5002, A ;output push pull 

    LD $5003, A ; see page 101

    ld a,#4

       ld $0x5000,a

    I don't know if are properly this value ld a,#4, Porta3 is the third 1, 2, 4

    carnett1
    carnett1Author
    Associate III
    Nov 22, 2010 7:33 PM UTC
    Posted on November 22, 2010 at 20:33

    Thank you - that was it.  I use 4 insted of 3

    charles

    infoinfo967
    Associate II
    Nov 23, 2010 6:51 PM UTC
    Posted on November 23, 2010 at 19:51

    What do you mean?

    Its an example, I mean If you want to get a port voltage outputs  for example

    cn1 pin4 is ground

    cn1 pin9 is porta3

    When you write a one in this bit, I thik you have a high output voltage

    between 4 and 9 you have in the multimeter screen 3,4 vdc.

    port a1 a2 a3 a4 a5 a6

           0   0   1   0  0   0

    I think you can write ld a,#4   (porta3=1)

    ¡¡¡Please we need a comunity expert revision data!!!

    spiovan9
    Associate III
    Dec 7, 2010 4:23 PM UTC
    Posted on December 07, 2010 at 17:23

    Hi all,

    even if yours is not the case, I'd like just to pay attention when using PE.2 and PE.3 port E pins, either as in or out: they're ''TRUE OPEN DRAIN''. It means that the pins don't have built-in pull-up resistors. Therefore reading in or writing out active level signals don't have effect too.

    In the STM8S105C datasheet page 22/127 the pin description have a small ''(T)'' aside that stands for ''True open drain''.

     

    Good work

     

    Stefano

     

     

     

     

    From: Aturate

    Posted: Tuesday, November 23, 2010 7:51 PM

    Subject: IO ports

    What do you mean?

    Its an example, I mean If you want to get a port voltage outputs  for example

    cn1 pin4 is ground

    cn1 pin9 is porta3

    When you write a one in this bit, I thik you have a high output voltage

    between 4 and 9 you have in the multimeter screen 3,4 vdc.

    port a1 a2 a3 a4 a5 a6

           0   0   1   0  0   0

    I think you can write ld a,#4   (porta3=1)

    ¡¡¡Please we need a comunity expert revision data!!!

    infoinfo967
    Associate II
    Dec 13, 2010 5:55 PM UTC
    Posted on December 13, 2010 at 18:55

    Dear Stefano,

    To obtain in cn3 pin out ''portb'' a sample example:

    steps of numbers from 0 to 1111111

    1=3,4vcc 0=gnd

    with configuration needs of ddr, cr1, cr2

    i have explained well?

    I program with asm.

    thank you