Skip to main content
Philipp Krause
Senior II
Jul 16, 2018 7:32 AM UTC
Question

Introducing more STM8 devices with low pin count?

Posted on July 16, 2018 at 09:32

ST has recently introduced 8-pin STM8 devices, while previously the lowest pin count available was 20.

I would like to see more STM8 devices with relatively low pin count, e.g. 12 or 14 pins. Since I intend to replace an Elan Microelectronics EM78P153A �C by an STM8, a compatible pinout would be great, but any 12- or 14-pin device would be good.

Are there any plans to introduce further STM8 devices with less than 20 pins?

Philipp

#stm8s001 #em78p153a #low-pin-count #new-device
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    Aug 8, 2018 1:52 PM UTC

    Bumping to remove from the home page (No Answer Posts)

    ST has sale staff/organization that can provide customers with forward looking and roadmap information. Call the local office, or your distributor

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..