Skip to main content
ST MICROCONTOLLER
Associate II
Dec 21, 2016 12:02 PM UTC
Question

Interrupt not working

Posted on December 21, 2016 at 13:02

I am trying to run a code in which timer causes an interrupt and everytime interrupt is generated, a variable h is incremented, but it remains zero in quickwatch window. My code is written below in stvd and cosmic compiler.

#include 'stm8s.h'

#include 'stm8s_tim1.h'

#include 'stm8s_itc.h'

#define TIM1_PSCRH (*(volatile uint8_t *)0x5260)

#define TIM1_CR1    (*(volatile uint8_t *)0x5250)

#define TIM1_ARRH    (*(volatile uint8_t *)0x5263)

#define TIM1_ARRL    (*(volatile uint8_t *)0x5264)

#define TIM1_PSCRL    (*(volatile uint8_t *)0x5261)

#define TIM1_IER (*(volatile uint8_t *)0x5254)

int h;

void main(void)

{

            //TIM1_SetCounter(5);enableInterrupts();GPIO_Config();

            //TIM1_DeInit();

TIM1_ARRH=0X55;

TIM1_ARRL=0X26;

TIM1_PSCRH = 0x3e;

TIM1_PSCRL = 0x80;

TIM1_CR1=0X81;

TIM1_IER=0X01;

enableInterrupts();

      while(1)

      {

        

       }

         }

INTERRUPT_HANDLER (TIM1_UPD_OVF_IRQHANDLER,23)

//@interrupt @far void TIM1_OVF_TRG_BRK_IRQ_Handler(void)

{

    h++;

}

    

#ifdef USE_FULL_ASSERT

/**

  * @brief  Reports the name of the source file and the source line number

  *   where the assert_param error has occurred.

  * @param file: pointer to the source file name

  * @param line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t* file, uint32_t line)

{

  /* User can add his own implementation to report the file name and line number,

     ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */

  /* Infinite loop */

  while (1)

  {

  }

}

#endif

What is wrong with the code? Kindly help me.

Thank you.

    This topic has been closed for replies.

    12 replies

    Schmidt.Andreas
    Explorer
    Dec 21, 2016 2:48 PM UTC
    Posted on December 21, 2016 at 15:48

    Hi,

    try to use : volatile int h;

    Regards

    Andreas

    ST MICROCONTOLLER
    Associate II
    Dec 22, 2016 7:10 AM UTC
    Posted on December 22, 2016 at 07:10

    Thanks, but declaring variable h as volatile didn't make any change.

    Seb
    ST Employee
    Dec 21, 2016 3:28 PM UTC
    Posted on December 21, 2016 at 16:28

    Are you using the debugger? 

    Is the code enabling timer internal clock so you can actually write the timer registers?

    In an old code, I've got this:

      CLK_PeripheralClockConfig(CLK_Peripheral_TIM1, ENABLE);

    Put as first step... (STM8L151)

    ==============================

    Digging at the std lib:

    void CLK_PeripheralClockConfig(CLK_Peripheral_TypeDef CLK_Peripheral, FunctionalState NewState)

    {

    /* Check the parameters */

    assert_param(IS_CLK_PERIPHERAL(CLK_Peripheral));

    assert_param(IS_FUNCTIONAL_STATE(NewState));

    if (((uint8_t)CLK_Peripheral & (uint8_t)0x10) == 0x00)

    {

    if (NewState != DISABLE)

    {

    /* Enable the peripheral Clock */

    CLK->PCKENR1 |= (uint8_t)((uint8_t)1 << ((uint8_t)CLK_Peripheral & (uint8_t)0x0F));

    }

    else

    {

    /* Disable the peripheral Clock */

    CLK->PCKENR1 &= (uint8_t)(~(uint8_t)(((uint8_t)1 << ((uint8_t)CLK_Peripheral & (uint8_t)0x0F))));

    }

    }

    else

    {

    if (NewState != DISABLE)

    {

    /* Enable the peripheral Clock */

    CLK->PCKENR2 |= (uint8_t)((uint8_t)1 << ((uint8_t)CLK_Peripheral & (uint8_t)0x0F));

    }

    else

    {

    /* Disable the peripheral Clock */

    CLK->PCKENR2 &= (uint8_t)(~(uint8_t)(((uint8_t)1 << ((uint8_t)CLK_Peripheral & (uint8_t)0x0F))));

    }

    }

    }

    and yes, you need to declare the variable as volatile to be sure.

    ST MICROCONTOLLER
    Associate II
    Dec 22, 2016 7:13 AM UTC
    Posted on December 22, 2016 at 07:13

    Thanks, I am using stm8s003k3 board with debugger, but the value of h is seen as 0 in simulator also.

    simon ferrer
    Associate
    Dec 21, 2016 10:08 PM UTC
    Posted on December 21, 2016 at 23:08

    Have you enabled the interrupt at NVIC Level?

    ST MICROCONTOLLER
    Associate II
    Dec 22, 2016 7:15 AM UTC
    Posted on December 22, 2016 at 07:15

    Thanks, do I have to edit any of the header files to enable interrupt at NVIC level?

    ST MICROCONTOLLER
    Associate II
    Dec 22, 2016 1:23 PM UTC
    Posted on December 22, 2016 at 14:23

    I have included stm8s_itc.h. I have seen somewhere stm8s_it.h file being included, which I think, is supported for raisonance as well as cosmic. When I include that file, another error takes place  'symbol f_NonHandeledInterrupt multiply defined'

    Thank you.

    Schmidt.Andreas
    Explorer
    Jan 5, 2017 8:55 AM UTC
    Posted on January 05, 2017 at 08:55

    Have you enabled the interrupts?

    enableInterrupts();  // usally before the main while loop...

    therefore you have to include: stm8l15x.h

    ramon13666
    Associate II
    Jan 9, 2017 7:55 AM UTC
    Posted on January 09, 2017 at 08:55

    TIM1_CR1=0X81;
    TIM1_IER=0X01;�?�?

    Change to

    TIM1_IER=0X01;
    TIM1_CR1=0X81;�?�?