Skip to main content
Mayank_07
Visitor II
November 26, 2024
Question

interfacing bosch bme688 sensor with Stm32

Hello,
I’m working on interfacing the Bosch BME688 sensor with my STM32 Nucleo-F446ZE development board using the BSEC library. The sensor is correctly providing temperature, pressure, humidity, and gas resistance data. However, I’m facing an issue when trying to calculate the IAQ (Indoor Air Quality).

The function bsec_do_steps() returns the following errors during debugging:

  • BSEC_E_DOSTEPS_VALUELIMITS
  • BSEC_I_DOSTEPS_NOOUTPUTSRETURNABLE

Here’s what I’ve done so far:

  1. Initialized the BME688 and configured it in forced mode using settings from bsec_sensor_control().
  2. Populated the bsec_input_t array with sensor data and called bsec_do_steps().
  3. Verified that timestamps and sensor signals are correctly passed.

Despite this, IAQ outputs are not generated. I suspect the issue might be related to input data limits or incorrect configuration, but I’m not sure how to resolve it.

Has anyone encountered similar errors or could provide guidance on resolving these issues?
Any help would be greatly appreciated!

Thanks in advance!

This topic has been closed for replies.

3 replies

Andrew Neil
Super User
November 26, 2024

@Mayank_07 wrote:

 The sensor is correctly providing temperature, pressure, humidity, and gas resistance data. !


So the problem is not in interfacing the sensor - that part is working fine?

 


@Mayank_07 wrote:

 using the BSEC library. 


This: https://www.bosch-sensortec.com/software-tools/software/bme680-software-bsec/ ?

That's Bosch's software - nothing to do with ST - you need to contact Bosch for support with their software.

https://community.bosch-sensortec.com/

 


@Mayank_07 wrote:

The function bsec_do_steps() returns the following errors during debugging:

  • BSEC_E_DOSTEPS_VALUELIMITS
  • BSEC_I_DOSTEPS_NOOUTPUTSRETURNABLE

So step into that function, and see what causes it to return those errors.

 

PS:

Also try googling those error names - this document refers to them, with suggested fixes:

https://git.digital-infinity.de/DigitalInfinity/ESP32-PaxCounter/raw/commit/17cd82da686440d9e41a3f8a2fab59e9441f43a0/lib/Bosch-BSEC/docs/BST-BME680-Integration-Guide-AN008-47.pdf

presumably it should be available direct from Bosh somewhere...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Strooom
Senior
July 24, 2025

Those errors are explained in the integration guide BST-BME-Integration-Guide-AN011-61.pdf

It's however not possible to debug/step through the code to find out why the errors occur, because the BSEC library is closed source and provided as a precompiled libalgobsec.a file...

 

Strooom
Senior
July 30, 2025

Hi @Mayank_07 , I have the IAQ working on a custom board with STM32L431.

It’s open source, but still work-in-progress. https://github.com/Strooom/BME688-ML-SW