Skip to main content
Associate
October 15, 2024
Question

Inquiry for WUXGA LCD Controller Chip Replacement

I hope this message finds you well.

I am currently looking for a WUXGA LCD controller chip. We have been using the FLI5962H-LF-AA and FLI5962H-LF, but these parts have been discontinued and are no longer available.

Could you please recommend a similar WUXGA LCD controller chip that meets the same specifications?

Thank you.

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
October 15, 2024

So 1920x1200 ?

That chip has a lot of functionality, and you need all of it, or just a subset?

A this point the markets probably with 4K/UHD capable stuff. Check what Fire sticks or Roku dongles are using.

Likely to be ARM/MIPS based than x86

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JASON_KIMAuthor
Associate
October 17, 2024

Thank you for your response.

The functionality we require is WUXGA (1920 × 1200) with DVI and HDCP support. Since this is for an older product, it seems that such specifications are not commonly available nowadays. However, we need an IC chip that is either similar or has better specifications. Additionally, the FLI5962H-LF-AA has 256 pins, so if there are no current options with 256 pins, I would appreciate any recommendations for modern alternatives.

Thank you again for your help!

JASON_KIMAuthor
Associate
October 17, 2024

Here is the data sheet for the Monitor Controller Chip from the respective manufacturer.

 
October 17, 2024

You can find suppliers who can provide you with samples and have them send them to you for use.