Skip to main content
boris239955
Associate II
Dec 6, 2005 4:30 AM UTC
Question

Information needed on STANDBY mode

Posted on December 06, 2005 at 05:30

Information needed on STANDBY mode

This topic has been closed for replies.

9 replies

boris239955
Associate II
Jul 22, 2005 1:07 PM UTC
Posted on July 22, 2005 at 15:07

Hi all,

There are a few things I'm not sure about regarding STANDBY mode.

The datasheet says ''All the I/Os belonging to the kernel are forced into High Impedance''. Does that mean ALL I/O pins, or are there exceptions (e.g. EMI, pins configured as Alternate Functions, etc.) ?

Also, it says that the system RAM is cleared. What happens to the internal registers ? Do they all retain their values, or are some reset to the default values (e.g. I/O pins config, clock config...) ?

Basically, I want to be able to power-down my system by software, and restart it with the WAKEUP pin. I'm thinking about doing the following :

* On power-down :

- switch to the 32 kHz oscillator

- power-down my external oscillator (connected to the CK pin)

- activate the STANDBY mode

* On wake-up :

- switch back to the external oscillator

- restart the program

Is this going to work as expected ?

Any info will be greatly appreciated !

:D

hichem2
Associate
Jul 26, 2005 7:38 AM UTC
Posted on July 26, 2005 at 09:38

Hello,

The STANDBY sequence is initiated either:

– by setting the PWRDWN bit in the PCU_PWRCR register (software STANDBY entry)

– or by externally forcing the nSTDBY pin to ‘0’ (hardware STANDBY entry).

Caution: You have to manage the nSTDBY, WAKEUP and RESET pin states in order to enter or exit STANDBY mode (refer to the STR71x reference manual, STANDBY section).

Cheers

Hich ;)

boris239955
Associate II
Jul 26, 2005 8:45 AM UTC
Posted on July 26, 2005 at 10:45

Hi Hich,

Thanks for your reply.

I understand how to initiate standby mode (I'll be using the software entry), but I'm still not sure about the high-impedance thing, and whether all registers values are preserved when restarting from standby.

I'm currently designing a protoype board, and I'll like to be sure that my understanding is correct before finalizing the PCB :)

hichem2
Associate
Jul 26, 2005 8:50 AM UTC
Posted on July 26, 2005 at 10:50

Hi Fizlo,

Core, memories and peripherals not powered by 1.8V internal supply.

Cheers,

Hich :D

boris239955
Associate II
Jul 26, 2005 9:02 AM UTC
Posted on July 26, 2005 at 11:02

Sorry to bother you again Hich,

So if I understand correctly your reply,

- All I/O pins switch to high-impedance

- All registers values are preserved

- Only the RAM is cleared

Right ? 8-)

hichem2
Associate
Jul 26, 2005 9:09 AM UTC
Posted on July 26, 2005 at 11:09

Hi,

Right, just All I/Os are forced to high impedance except the Standby I/Os(nSTDBY, nRSTIN, WAKEUP, RTCXTI and RTCXTO.).

ciao,

hich

boris239955
Associate II
Jul 26, 2005 9:29 AM UTC
Posted on July 26, 2005 at 11:29

Thank you very much, Hich ! :D

hichem2
Associate
Jul 28, 2005 4:46 AM UTC
Posted on July 28, 2005 at 06:46

Hi,

You are welcome.

Cheers,

Hich :p

hichem2
Associate
Dec 6, 2005 4:30 AM UTC
Posted on December 06, 2005 at 05:30

Hi,

After wake-up from the standby mode only the RTC data are preseved, RAM and all the others peripherals data are cleared.

Best regatds,

Hich 8-)