Skip to main content
vince
Associate III
Apr 1, 2014 7:04 PM UTC
Question

Infinite ISR on STM8L

Posted on April 01, 2014 at 21:04

I'm exploring an STM8L152 on the Discovery Board. That board has a user button, which I have set to trigger an interrupt on a GPIO (pin C1, if that matters). I can watch the interrupt fire in the debugger (using STVD), and right now my ISR has only the disableInterrupt() command and return. The ISR never exits, though, looping continuously. I have not had this problem on an STM8S105. Does anyone have some insight into what might be going on? Thanks.

[UPDATE - Guys, never mind. It looks like on these machines you must manually clear a pending external interrupt flag via the EXTI->SR1 register, unlike on some other 8's, which have no flags. Then, by some perverse logic, clearing the bit actually means writing a ''1''.]

#stm8l #external-interrupt
This topic has been closed for replies.