Skip to main content
igorl
Associate III
Oct 21, 2003 6:13 PM UTC
Question

In-System JTAG Debugger for uPSD32xx

Posted on October 21, 2003 at 20:13

In-System JTAG Debugger for uPSD32xx

This topic has been closed for replies.

2 replies

joseph2399
Associate II
May 17, 2011 9:56 AM UTC
Posted on May 17, 2011 at 11:56

Yes, ST and Keil developed a JTAG debugger called ULINK (under $200), however, it is for debugging the Turbo uPSD 33xx family processors. You can find more information on ULink at:

http://www.keil.com/ulink

.

As far as for uPSD32xx family, you can obtain emulator from Nohau, which is more pricy but works very well, or you can use a lower cost emulator from Manley ~$200 but some of the fuctions are not yet supported, such as memory tracing and memory paging. You can get additional information on Manley ME3200 at:

http://www.manley.com.cn/english

igorl
igorlAuthor
Associate III
May 17, 2011 9:56 AM UTC
Posted on May 17, 2011 at 11:56

Hello!

Another question concerning uPSD. I have the information from 3rd party developing company, that ST was to produce a JTAG debugger which costs only 100-200$. This part was proposed to use the same Flash-link interface as it uses now for ISP.

Will you answer, when is this part is availible?

Thank you very much in advance.