Skip to main content
jas
Associate III
Feb 8, 2007 7:23 PM UTC
Question

In circuit bootloader via RS232 or USB ?

Posted on February 08, 2007 at 20:23

In circuit bootloader via RS232 or USB ?

This topic has been closed for replies.

33 replies

twinknight
Associate II
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

use STR750F

shangdawei1
Associate III
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

any news about the source files for the DFU ?

najoua
Associate
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

Hello Vendelin,

Bank0 is remapped to address 0x80000 using CAPS and Bank1 size is 32Kbytes as you said.

Regards,

Najoua.

[ This message was edited by: Najoua on 07-02-2007 09:57 ]

vaclav2
Associate II
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

Hi

I read pdf file about UART bootloader and I have one question. Is the start adress of bank 0 after remaping by CAPS 0x80000 or 0x8000? Bank1 has only 32kB adress space.

Best regards

Vendelin

vaclav2
Associate II
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

Hi

I read pdf file about UART bootloader and I have one question. Is the start adress of bank 0 after remaping by CAPS 0x80000 or 0x8000? Bank1 has only 32kB adress space.

Best regards

Vendelin

sr_shinde2
Associate
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

Hi All,

Will This bootloader work for STR912FAW46 ?

Regards

Sai

ron2
Associate
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

I was just reading an article in embedded-Developer.com. Here is the link.

http://www.embedded-developer.com/tools/470/STMicroelectronics/um0290.htm

It says that the USB Boot loader called a DFU. What does DFU stand for?

Is available in the USB developer kit.

I haven't checked it out yet but it is something I need for my project.

:D

davidwilson9
Visitor II
Jun 28, 2011 7:44 AM UTC
Posted on June 28, 2011 at 09:44

Where is the link to download?

Tesla DeLorean
Guru
Jun 28, 2011 6:47 PM UTC
Posted on June 28, 2011 at 20:47

Where is the link to download?

AWOL

The thread is from 2006/2007, a prior incarnation of the forum, and user database. The current forum had a meltdown in mid May 2011. Attachments have not survived these processes, ST might be able to dig them out of the archives, but that's not certain. You may want to check if the material is mirrored other places on the net, or that the posters are active on other forums.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pantuca.Erwin
Visitor II
Jun 30, 2011 2:36 AM UTC
Posted on June 30, 2011 at 04:36

previously i had been able to find a lot of very usefule files (application notes, sample source, tools, utilities etc) for the str9.  now i could not find these same files in their new website layout.  does it mean they are gone?  because we dont usually download all of these as they are easily available (and searchable) before.  that would be a very big concern for us regarding using str9 and st mcu in general?