Skip to main content
bruno239955_stm1_stmicro
Associate III
Oct 6, 2009 11:19 AM UTC
Question

Impossible to use ADC on several channels (repost)

Posted on October 06, 2009 at 13:19

Impossible to use ADC on several channels (repost)

    This topic has been closed for replies.

    1 reply

    bruno239955_stm1_stmicro
    Associate III
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    Hi,

    Something goes wrong with the forum. Please discard my previous message and read this one:

    I am writing an application with STM8S208RB on the Raisonance REva evaluation board. I read analog values from entries IN1, IN2, potentiometer and temperature sensor (on PF4-7).

    I use single conversion, no IT, no Schmidt trigger. Everything is simple, except that I need to be able to read any one of the entries above when I need it.

    I wrote a simple application that does just that, but the values that I read from the ADC change in an inconsistent manner. I spent quite some time trying to understand what happens, and the ST library examples work well.

    Following is the faulty code. I attach a zip file with the Ride7 project so that you can experiment wil the full project.

    Can anyone see what is the problem?

    Thanks for your Help,

    Bruno

    #include

    #include ''stm8s.h''

    /**

    * Analog I/Os are as follows on the STM8S208 daughterboard:

    * IN1 PF.4 - External analog input

    * IN2 PF.5 - External analog input

    * TEMP PF.6 - Temperature sensor analog input

    * POT PF.7 - Potentiometer analog input, min=0V, max=VDD

    */

    #define CHANNEL_IN1 ADC2_CHANNEL_12

    #define CHANNEL_IN2 ADC2_CHANNEL_13

    #define CHANNEL_TEMP ADC2_CHANNEL_14

    #define CHANNEL_POT ADC2_CHANNEL_15

    #define MAX_ADC_VAL 0x3FF /* 10-bit ADCs */

    /**

    * Voltage (in mV) of the Vcc of the Daughterboard.

    * This (global) variable is used in the voltage conversions from the ADC

    * for the conversion between the ADC range to the required voltage.

    * The default value is 4700 (4.7V).

    */

    unsigned short VDDmV = 4700;

    /**

    * @brief Initializes ADC2 inputs for PF.4-7

    * @param None

    * @retval None

    */

    void ADC_Init(void)

    {

    /* Init GPIO for ADC2 */

    GPIO_Init(GPIOF, GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7, GPIO_MODE_IN_FL_NO_IT);

    /* ADC2 configuration */

    ADC2_DeInit();

    /* Disable interrupts */

    ADC2_ITConfig(DISABLE);

    }

    /**

    * Read the value from a given channel

    * @param channel The channel number to read from

    * @retval The analog value read (in mV)

    */

    unsigned short ADC_ReadChannel(unsigned char channel)

    {

    unsigned short val;

    /* Configure ADC2 for a single capture on given channel */

    ADC2_Init(ADC2_CONVERSIONMODE_SINGLE,

    channel,

    ADC2_PRESSEL_FCPU_D2,

    ADC2_EXTTRIG_TIM,

    DISABLE,

    ADC2_ALIGN_RIGHT,

    channel,

    DISABLE);

    ADC2_Cmd(ENABLE);

    ADC2_StartConversion();

    /* Wait for end of conversion */

    while(ADC2_GetFlagStatus() == RESET)

    ;

    val = ADC2_GetConversionValue();

    ADC2_Cmd(DISABLE);

    ADC2_ClearFlag();

    return val;

    }

    void main(void)

    {

    ADC_Init();

    while(1)

    {

    printf(''I1 = %04x '', ADC_ReadChannel(CHANNEL_IN1));

    printf(''I2 = %04x '', ADC_ReadChannel(CHANNEL_IN2));

    printf(''POT = %04x '', ADC_ReadChannel(CHANNEL_POT));

    printf(''TEMP = %04x\n'', ADC_ReadChannel(CHANNEL_TEMP));

    }

    }