Skip to main content
Associate
Jan 26, 2026 7:45 AM UTC
Solved

Identify this part?

Edited to place the image in the post - for easier viewing.


Hello,
This is my first time posting.
I am trying to find the P/N from the part's marking.
If you know it, please let me know.

Engraving: GP229

Guess: Schottky barrier diode STPS2L60 - 2A, 60V. Is that correct...?

If you have any information, please let me know. Thank you.

 

AndrewNeil_0-1769438378563.jpeg

 

CXTURBOBest answer
Associate
Feb 5, 2026 6:32 AM UTC

Sorry for the late reply.
I obtained two candidate types and made a decision.
In the end, it appears that STTH112 was the correct answer.
STTH112 does not conduct current even at 1KV or reverse voltage, but STTH102 did.
Now I can install it with confidence.
Thank you for your advice.

9 replies

AScha.3
Super User
Jan 26, 2026 8:27 AM UTC

Hi,

marking could be ... GU

AScha3_0-1769416008969.png

Look, what it should do probably in the board : diode or ESD protection ?

If you feel a post has answered your question, please click on " Best Answer ".
CXTURBOAuthor
Associate
Jan 27, 2026 5:19 AM UTC

Thank you for getting in touch.
I repair faulty power supplies, circuit boards, etc. that are entrusted to me by customers.
In this case, I needed this diode to repair an AC servo driver.
As I don't have a circuit diagram, I don't know its purpose (protection, ESD, etc.).
I plan to create a circuit diagram depending on the situation, but I was in a difficult situation as I couldn't install an uncertain part.
Is it likely that the SM6T200A mentioned in your comments is the P/N?
Also, is there a way to identify the P/N from the engraving?
Thank you in advance.

 

Please excuse any strange notation as I am using Japanese translation software.

CXTURBOAuthor
Associate
Jan 27, 2026 5:32 AM UTC

I'm sorry I don't really understand how to use it.
Regarding the STTH102/112, as advised by Peter, I'd like to remove the parts and measure them.
I'll comment once I've finished checking.
Thank you in advance.

Peter BENSCH
ST Technical Moderator
Jan 26, 2026 9:09 AM UTC

Welcome @CXTURBO , to the community!

You'll find the marking in the 2nd line, i.e. U12.

Unfortunately, the marking is ambiguous and could refer to either STTH102 (Utrafast 200V) or STTH112 (Utrafast 1.2kV) , which differ significantly from the blocking voltage and the forward voltage. For a successful replacement, you should therefore try to find out what the maximum voltage can be.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.