Skip to main content
upamir2
Associate II
Apr 17, 2007 5:41 AM UTC
Question

ICC Cable Length

Posted on April 17, 2007 at 07:41

ICC Cable Length

This topic has been closed for replies.

5 replies

upamir2
upamir2Author
Associate II
Apr 6, 2007 8:08 AM UTC
Posted on April 06, 2007 at 10:08

Have a good day

The icc cable between programmer and PCB, How long can it be.(maximum without mistake)

İ use reva board v1 and st7fliteus5

laurent239955_stm1
Associate
Apr 16, 2007 1:00 PM UTC
Posted on April 16, 2007 at 15:00

Hello,

one ICC cable is provided with Reva starter kit. Raisonance is sure that

it works with it but doesn't give any guarantee for longer one because

they didn't make serious test (stress) on that feature. For information,

ST made some Lite09 programming tests with Stick and different ICC cable

length four years ago. No problem has been found with 30cm, 1m, 2m and

3m cables.

It doesn't mean results are identical with RLink, it depends on PC and

environment, i recommend you to make some tests.

Best regards

Pascal

upamir2
upamir2Author
Associate II
Apr 17, 2007 3:20 AM UTC
Posted on April 17, 2007 at 05:20

Have a good day

are the test cables longer than 1m shielded.

i use not shielded 60cm and sometimes ''there is no mcu''.

thanks for your interest

laurent239955_stm1
Associate
Apr 17, 2007 5:37 AM UTC
Posted on April 17, 2007 at 07:37

Hi,

The ST-STICK is different comparing with the R-Link : STICK is plugged through parallel port with only passive components but R-Link is connected through USB and there is a ST7 onside the Rlink to interface between USB and ICC connection.

Raisonance guarantee only with the ICC cable provided, but you have also to take care about the length on your PCB itself.

Anyway, are you sure that no error will occur with a smaller ICC cable.

Depending on your constraint you can rather increase the USB cable length.

Best regards

Laurent

upamir2
upamir2Author
Associate II
Apr 17, 2007 5:41 AM UTC
Posted on April 17, 2007 at 07:41

nearly 40 cm is ok.

Thanks for your interest