Skip to main content
harshvardhan
Visitor II
Dec 18, 2014 10:03 AM UTC
Question

IAP bootloader source code for STM8S

Posted on December 18, 2014 at 11:03

I�m going through this application note on the ST website: http://www.st.com/web/en/catalog/tools/PF258002

The application note states that it comes with source code for an example of an IAP bootloader implementation: 

�For this purpose, an example of a user-bootloader firmware is provided with this application note. This package is divided into three main subdirectories, each one dedicated to one STM8 family member: STM8AF, STM8L and STM8S. For the STM8AL family, please use the STM8L directory. Each directory is composed of the following components: 

? Sources: containing the firmware source code�

However, the download link on the same page (STSW-STM8062) only has S19 hex files and no source code. 

I was wondering if someone could provide me with the source code. Any help would be appreciated.

#stm8 #bootloader #iap #stsw-stm32098
This topic has been closed for replies.