Skip to main content
igorl
Associate III
April 13, 2004
Question

I2C with uPSD3212

  • April 13, 2004
  • 2 replies
  • 722 views
Posted on April 13, 2004 at 10:43

I2C with uPSD3212

This topic has been closed for replies.

2 replies

joseph2399
Associate II
May 17, 2011
Posted on May 17, 2011 at 11:59

We are working to release a uPSD3200 I2C driver that will be made available on our website (target release is within a month). A notification will be made on the forum when it is available.

On a case-by-case basis, a beta version of the I2C driver will be made available. If interested in receiving a copy of the beta version, please send a request to

mailto:apps.psd@st.com

with the following information:

Name

Company Name

Phone Number

Location (City, State, Country)

uPSD part number of device being used (3234, 3254, etc.)

Application

Projected annual volume (units)

Regards,

uPSD Applications Engineering

igorl
igorlAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:59

Dear all!

Can anybody help me? I tried to used I2C and came across with one problem: I set SII, then I set STA bit (start condition), then I load S2DAT register and it sends this 8-byte serie. But after it, both SDA and SCL are in ''0'' state, while they need to be at ''high-impedance'' state.

No device is connected to I2C from another side (uPSD3212 is the only device) and interrupts are disabled. Can we try I2C in such condition? Do you have any ASM-code exampple of I2C usage?

Thank you in advance.