Skip to main content
EBogo.1
Associate
April 21, 2020
Question

I2C slave configuration for STM8S208RBT6

Hello, I am trying to use STM8S208RBT6 as an I2C slave. It seems to be configured correctly, yet it doesn't acknowledge its address, and it doesn't get an interrupt. The registers are as follows:

PE_DDR = 0x20;

PE_ODR = 0x20;

PE_CR1 = 0x20;

PE_CR2 = 0x20;

I2C_CR1 = 0x01;

I2C_CR2 = 0x04;

I2C_FREQ = 0x10;

I2C_OARL = 0x28;

I2C_OARH = 0x40;

I2C_ITR = 0x02;

I2C_CCRL = 0x50;

I2C_CCRH = 0x00;

I2C_TRISER = 0x11;

I2C_PECR = 0x00.

What am I missing?

Thank you,

Eric.

    This topic has been closed for replies.

    1 reply

    EBogo.1
    EBogo.1Author
    Associate
    April 21, 2020

    OK, it turns out the problem is in the stm8s_i2c.c file provided by the ST. The initialization function in that file writes the I2C 7-bit address into the OARL register as it is, without accounting for the bit 0 of the OARL register. But it needs to shift the 7-bit address left by 1 bit. Thus, the address 0x28 becomes 0x50, and that is what needs to written into OARL. With this change I2C works.