Skip to main content
rgovindappa9
Associate II
Mar 24, 2011 11:00 AM UTC
Question

I2C protocol STOP condition not detected in slave-transmission mode

Posted on March 24, 2011 at 12:00

I2C protocol STOP condition not detected in slave-transmission mode

    This topic has been closed for replies.

    4 replies

    rgovindappa9
    Associate II
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Here is my Slave transmitter part in 

    @far @interrupt void I2C_IRQHandler(void)  /* I2C Interrupt handler*/

    is as follows

    /*SLAVE TRANSMITTER*/

    /*Data transmited from slave to master*/

    /*EV3-1: TxE=1, shift register empty, data register empty, write DR register.*/

    if(I2C_CheckEvent(I2C_EVENT_SLAVE_BYTE_TRANSMITTED))

      {

    /*Acknowledge failure*/

    /*EV3-2: AF=1, AF is cleared by writing ‘0’ in AF bit of SR2 register*/

    if(I2C_CheckEvent(I2C_EVENT_SLAVE_ACK_FAILURE))

    {

    I2C_ClearFlag(I2C_FLAG_ACKNOWLEDGEFAILURE);

    }

    /*EV3: TxE=1, cleared by writing DR; shift register not empty*/

    I2C_SendData(SomeData);

    I2C_ClearFlag(I2C_FLAG_TRANSFERFINISHED);

    }

    rgovindappa9
    Associate II
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    I am struggling for the last one week and have tried various combinations and permutations and have ran out of ideas - I have a requirement to implement Master-receiver and Slave-transmitter as interrupt state machines as outlined by the STM8S datasheet, polling is not an option. Any help will be highly appreciated

    rgovindappa9
    Associate II
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    The ACK failure is triggered in the slave when master sets ACK bit to 0

    rgovindappa9
    Associate II
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Here is Master-receiver implementation in I2C interrupt service routine

     /*MASTER RECEIVER, read-write byte=1*/

      else if(I2C_CheckEvent(I2C_EVENT_MASTER_BYTE_RECEIVED))

      {

      /*EV7_1: RxNE=1, cleared by reading DR register, program ACK=0 and STOP request*/

      if(SECOND_LAST_BYTE)

      {

       I2C_AcknowledgeConfig(I2C_ACK_NONE);

       I2C_CurrentReadData = I2C_ReceiveData(); 

      }  

      else if(LAST_BYTE)

      {

       I2C_CurrentReadData = I2C_ReceiveData();

       I2C_GenerateSTOP(ENABLE);

      }

      //EV7: RxNE=1, cleared by reading DR register

      else

      {  

       I2C_CurrentReadData = I2C_ReceiveData();

      }

      I2C_ClearFlag(I2C_FLAG_RXNOTEMPTY);  

     }