Skip to main content
ludo98
Associate II
Jul 4, 2006 12:01 PM UTC
Question

I2C interrupt

Posted on July 04, 2006 at 14:01

I2C interrupt

This topic has been closed for replies.

2 replies

ludo98
ludo98Author
Associate II
Jun 22, 2006 11:39 AM UTC
Posted on June 22, 2006 at 13:39

hello,

i have an problem with my RX_TX_Interrupt.

i am trying to write data toward an I2C slave.

The procedure is the following:

1. i initialise my I2c with the ITE bit set

2. my task send a Start condition

3. the interrupt ITERR occurs

4. read SB bit and send the adress:

if (I2C_FlagStatus ( desc->i2c, desc->access, I2C_SB)==SET){

// Envoi de l'adresse

desc->adresse&=~0x01;

desc->i2c->DR=(u8)desc->adresse;

}

5. the 2nd ITERR interrupt occurs

6. read ENDAD bit , Clear and send the data

if (I2C_FlagStatus ( desc->i2c,desc->access, I2C_ENDAD)==SET){

desc->write.numero_auto=2;

I2C_FlagClear (desc->i2c, I2C_ENDAD);

I2C_ByteSend(desc->i2c,desc->write.buffer[desc->write.pos]);

}

7. the RX_TX interrupt occurs

8. read BTF bit and send the second data:

if (desc->i2c->SR1 & 0x08) {

desc->write.pos++;

if (desc->write.pos ==(desc->write.len)){

desc->write.numero_auto = 3;

}

I2C_ByteSend(desc->i2c,desc->write.buffer[desc->write.pos]);

indices++;

}

REPEAT step 7 and 8 if you have more data

9. the RX_TX interrupt occurs

10.the Stop condition is send

if (desc->i2c->SR1 & 0x08) {

I2C_STOPGenerate (desc->i2c, ENABLE);

desc->write.numero_auto = 0;

indices++;

}

the problem is: th 1st IT TX_RX occurs when the bit

BTF is unset and after a litte delay the bit in the SR1 register is set. After the datasheet of STR712 the condition which permit to the interrupt to occur is when BTF an ITE are SET.

Have you an explain about this operating?

thanks

Ludo

llebotlan
Associate II
Jul 4, 2006 12:01 PM UTC
Posted on July 04, 2006 at 14:01

Thank you,

ludo78 is not here any more but I pursue their investigations.

I will have a look to your project.

Thanks,

Ludo