Skip to main content
AZama.693
Visitor II
April 13, 2020
Question

I2C gets stuck at EV8 I2C Event (I2C_EVENT_MASTER_BYTE_TRANSMITTING)

I am trying to get SMbus communication to work and it works fine most of the time but I have seen that after sometime it gets stuck at I2C event I2C_EVENT_MASTER_BYTE_TRANSMITTING.

I have implemented a timeout function which retries event 255 times but I can still see that the return I get from the I2C retry event is an error. I also tried to do MCU reset and re init I2C if it still gets stuck after timeout but then the mcu is resetting all the time.

Is my I2C_EventRetry function incorrect > Or is there any good way to handle this error?

Below is my Init, Transmit and Event Retry function.

void I2C_Init()
{
 /* Initialize I2C peripheral */
 I2C_Init(I2C1, I2C_SPEED, 0x00,
 I2C_Mode_SMBusHost, I2C_DutyCycle_2,
 I2C_Ack_Enable, I2C_AcknowledgedAddress_7bit); // 0x00 is a dummy value. Only used in slave mode
					 
	I2C_Cmd(I2C1, ENABLE); // Enable peripheral
}
 
static void I2C_EventRetry(I2C_Event_TypeDef I2C_Event)
{
	uint8_t retryCounter = 0;
	do{
 Delay_Us(1); 
 retryCounter++;
	}while((!I2C_CheckEvent(I2C1, I2C_Event)) && (retryCounter < RETRY_LIMIT)); 
}
 
static void StartTransmit(uint8_t slaveAddress, uint8_t commandCode, uint8_t dataLength, uint8_t regAddress1, uint8_t regAddress2)
{
	/* Disable I2C acknowledgement */
	I2C_AcknowledgeConfig(I2C1, ENABLE);
	
 /* Send I2C START condition */
 I2C_GenerateSTART(I2C1, ENABLE);
 
 /* Test on I2C EV5 and clear it */
	I2C_EventRetry(I2C_EVENT_MASTER_MODE_SELECT);
 
 /* Send slave address for write */
 I2C_Send7bitAddress(I2C1, slaveAddress, I2C_Direction_Transmitter);
 
 /* Test on I2C EV6 and clear it */
	I2C_EventRetry(I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED);
	
 /* Send the command code */
 I2C_SendData(I2C1, commandCode); 
 
 /* Test on I2C EV8 and clear it */
	I2C_EventRetry(I2C_EVENT_MASTER_BYTE_TRANSMITTING);
 
	/* Send the Data length */
 I2C_SendData(I2C1, dataLength); 
 
 /* Test on I2C EV8 and clear it */
	I2C_EventRetry(I2C_EVENT_MASTER_BYTE_TRANSMITTING);
	/* Send the Data byte */
 I2C_SendData(I2C1, regAddress1); 
 
 /* Test on I2C EV8 and clear it */
	I2C_EventRetry(I2C_EVENT_MASTER_BYTE_TRANSMITTING);
	/* Send the Data byte */
 I2C_SendData(I2C1, regAddress2); 
 
 /* Test on I2C EV8 and clear it */
	I2C_EventRetry(I2C_EVENT_MASTER_BYTE_TRANSMITTED); //EV8_2
/* Send Stop condition */
	I2C_GenerateSTOP(I2C1, ENABLE);
	Delay_Ms(1);
 
	 /* Send I2C START condition */
 I2C_GenerateSTART(I2C1, ENABLE);
 
 /* Test on I2C EV5 and clear it */
	I2C_EventRetry(I2C_EVENT_MASTER_MODE_SELECT);
 
 /* Send slave address for write */
 I2C_Send7bitAddress(I2C1, slaveAddress, I2C_Direction_Transmitter);
 
 /* Test on I2C EV6 and clear it */
	I2C_EventRetry(I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED);
 
	/* Send the command code */
 I2C_SendData(I2C1, commandCode); 
 
 /* Test on I2C EV8 and clear it */
	I2C_EventRetry(I2C_EVENT_MASTER_BYTE_TRANSMITTED); //EV8_2
		/* Send Stop condition */
	I2C_GenerateSTOP(I2C1, ENABLE);
}

    This topic has been closed for replies.