Skip to main content
Ali Kari
Associate
May 6, 2021
Question

I want to know what is the maximum pulse frequency that can be counted by stm8s003f3p6 .

My program is as described in stm8s reference manual 17.4.3 External clock source mode 1

and pulse counting is done in pin PC7 using HSI 16 Mhz , but the speed of counting is very low , for example for a 10 mhz pulse in 1 ms TIM1_CNTRL counts to 60 .

I want to know is this speed of counting correct ?

I want to make a frequency counter and need to have more speed to count high frequency wave . now it is possible to count up to 200 mhz pulse but resolution is very bad due to low speed of timer1 pulse counting .

As I said for 10 mhz pulse , counter is 60 so each increment of counter is equal to 10Mhz/60 = 167 khz .

my code for timer counter is as follows

#include <iostm8S003f3.h>

#include <intrinsics.h>

unsigned long int fr=0,f=0;  // fr increment in timer1 overflow , f is number of final pulse counting 

unsigned char h; //dummy variable 

int main(void)

{

  __disable_interrupt();  

  InitialiseSystemClock();

  InitialisePorts();

   

  config_counter();

  TIM1_IER_UIE = 1;  // enable timer 1 interrupt     

  __enable_interrupt();

   

  while (1)

  {

  

    fr=0;

     

    TIM1_CNTRH = 0; //reset counter 

    TIM1_CNTRL = 0;

    TIM1_CR1_CEN=1; // start counting

    delayms(1);

    TIM1_CR1_CEN=0; // stop counting 

    // calculate counter as a number = TIM1_CNTRH*256 + TIM1_CNTRL + fr*65536 

    // fr will increment whenever tim1 counter overflows 

    h=TIM1_CNTRH ;  

    f=h*256;

    h=TIM1_CNTRL;

    f=f+h;

    f=fr*65536+f;

       

  }

}

void delayms(int t)

{

 int d;

 while(t--)

 for (d = 0; d < 2020; ++d) ; //approximately 1 ms delay with 16 mhz clock 

}

#pragma vector = TIM1_OVR_UIF_vector

__interrupt void TIM1_UPD_OVF_IRQHandler(void)

{

 fr++;

 TIM1_SR1_UIF = 0; 

}

void InitialisePorts()

{

  PC_DDR_DDR7=0;  // pc7 as input 

  PC_CR1_C17 = 0; // no pullup 

  PC_CR2_C27 = 0; // no interrupt

}

void InitialiseSystemClock()

{

  CLK_ICKR = 0;            // Reset the Internal Clock Register.

  CLK_ICKR_HSIEN = 1;         // Enable the HSI.

  CLK_ECKR = 0;            // Disable the external clock.

  while (CLK_ICKR_HSIRDY == 0);    // Wait for the HSI to be ready for use.

  CLK_CKDIVR = 0;           // Ensure the clocks are running at full speed.

  CLK_PCKENR1 = 0xff;         // Enable all peripheral clocks.

  CLK_PCKENR2 = 0xff;        

  CLK_CCOR = 0;            // Turn off CCO.

  CLK_HSITRIMR = 0;          // Turn off any HSIU trimming.

  CLK_SWIMCCR = 0;          // Set SWIM to run at clock / 2.

  CLK_SWR = 0xe1;           // Use HSI as the clock source.

  CLK_SWCR = 0;            // Reset the clock switch control register.

  CLK_SWCR_SWEN = 1;         // Enable switching.

  while (CLK_SWCR_SWBSY != 0);    // Pause while the clock switch is busy.

}

void config_counter(){

 TIM1_CNTRH = 0;

 TIM1_CNTRL = 0; //Reset counter

 TIM1_IER = 0; //Interrupt disabled

 TIM1_SR1 = 0; //Clear Interrupt

 TIM1_CCMR2 |= 1<<0; //External pulse source T1C2

 TIM1_CCER1 &= ~(1<<5); //Rising edge

 TIM1_SMCR |= (7<<0); //External Clock Source

 TIM1_SMCR |= (6<<4); //T1C2 Input Source

 TIM1_CR1 &= ~(1<<0); //Counter disabled

 return;

}

    This topic has been closed for replies.

    4 replies

    WilkoL
    Senior
    May 7, 2021

    Any input signal has to be synchronized with the internal clock. In RM0016 page 191 you can read that:

    ---

    The ETRP frequency must be, at most,1/4 of fMASTER frequency. A prescaler can be enabled to

    reduce ETRP frequency. It is useful when inputting fast external clocks.

    ---

    So if your internal clock is 16 MHz, the maximum input frequency is 4 MHz. This is (probably) valid or every input to every peripheral, don't go any higher than 1/4 of the internal clock.

    Ozone
    Principal
    May 7, 2021

    I would suggest an external prescaler, like a highspeed equivalent to the 74LS68/74LS69, 74x90/74x93. or 74x160..163.

    WilkoL
    Senior
    May 7, 2021

    That would be the 74HC series, such as the 74HC390 (dual decade) or the 74HC393 (dual 4-bit binary riplle counter) The 74LS series need 5V to work, the 74HC will work as low as 2V although then they aren't very fast anymore. At 3.3V a frequency of 10 MHz will work fine.