Skip to main content
Ocohe
Associate
May 5, 2019
Question

i set timer1 channel1 registers as the same as timer1 channel 2,3,4 but it does'nt work

..

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    May 5, 2019

    Ok, and how do you think the cause can be determined with that level of detail? ​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Ocohe
    OcoheAuthor
    Associate
    May 6, 2019

    i uses the spl from the st.com for stm8s-discuvery with the 7 pwm example for timer 1 .

    after calling the function i can read in the debugger the next register value , it looks like ok i think but not working

    this example set pwm in timer 1 2 3 4

    2,4 works , 1 does'nt work.

    TIM1->CCRE1 = 0x77

    TIM1->CCMR1 = 0x70

    TIM1->OISR = 0x5F

    TIM1->CR1 = 0x01

    TIM1->BKR = 0x80

    in the main() file :

      TIM1_TimeBaseInit(0, TIM1_COUNTERMODE_UP, 4095, 0);

       TIM1_OC1Init(TIM1_OCMODE_PWM2, TIM1_OUTPUTSTATE_ENABLE, TIM1_OUTPUTNSTATE_ENABLE,

            CCR2_Val, TIM1_OCPOLARITY_LOW, TIM1_OCNPOLARITY_HIGH, TIM1_OCIDLESTATE_SET,

            TIM1_OCNIDLESTATE_RESET);

    in the tim1.c file

    void TIM1_TimeBaseInit(uint16_t TIM1_Prescaler,

                TIM1_CounterMode_TypeDef TIM1_CounterMode,

                uint16_t TIM1_Period,

                uint8_t TIM1_RepetitionCounter)

    {

     /* Check parameters */

     assert_param(IS_TIM1_COUNTER_MODE_OK(TIM1_CounterMode));

      

     /* Set the Autoreload value */

     TIM1->ARRH = (uint8_t)(TIM1_Period >> 8);

     TIM1->ARRL = (uint8_t)(TIM1_Period);

      

     /* Set the Prescaler value */

     TIM1->PSCRH = (uint8_t)(TIM1_Prescaler >> 8);

     TIM1->PSCRL = (uint8_t)(TIM1_Prescaler);

      

     /* Select the Counter Mode */

     TIM1->CR1 = (uint8_t)((uint8_t)(TIM1->CR1 & (uint8_t)(~(TIM1_CR1_CMS | TIM1_CR1_DIR)))

                | (uint8_t)(TIM1_CounterMode));

      

     /* Set the Repetition Counter value */

     TIM1->RCR = TIM1_RepetitionCounter;

    }

    void TIM1_OC1Init(TIM1_OCMode_TypeDef TIM1_OCMode,

             TIM1_OutputState_TypeDef TIM1_OutputState,

             TIM1_OutputNState_TypeDef TIM1_OutputNState,

             uint16_t TIM1_Pulse,

             TIM1_OCPolarity_TypeDef TIM1_OCPolarity,

             TIM1_OCNPolarity_TypeDef TIM1_OCNPolarity,

             TIM1_OCIdleState_TypeDef TIM1_OCIdleState,

             TIM1_OCNIdleState_TypeDef TIM1_OCNIdleState)

    {

      

     /* Disable the Channel 1: Reset the CCE Bit, Set the Output State , 

     the Output N State, the Output Polarity & the Output N Polarity*/

     TIM1->CCER1 &= (uint8_t)(~( TIM1_CCER1_CC1E | TIM1_CCER1_CC1NE 

                   | TIM1_CCER1_CC1P | TIM1_CCER1_CC1NP));

     /* Set the Output State & Set the Output N State & Set the Output Polarity &

     Set the Output N Polarity */

     TIM1->CCER1 |= (uint8_t)((uint8_t)((uint8_t)(TIM1_OutputState & TIM1_CCER1_CC1E)

                       | (uint8_t)(TIM1_OutputNState & TIM1_CCER1_CC1NE))

                  | (uint8_t)( (uint8_t)(TIM1_OCPolarity & TIM1_CCER1_CC1P)

                        | (uint8_t)(TIM1_OCNPolarity & TIM1_CCER1_CC1NP)));

      

     /* Reset the Output Compare Bits & Set the Output Compare Mode */

     TIM1->CCMR1 = (uint8_t)((uint8_t)(TIM1->CCMR1 & (uint8_t)(~TIM1_CCMR_OCM)) | 

                 (uint8_t)TIM1_OCMode);

      

     /* Reset the Output Idle state & the Output N Idle state bits */

     TIM1->OISR &= (uint8_t)(~(TIM1_OISR_OIS1 | TIM1_OISR_OIS1N));

     /* Set the Output Idle state & the Output N Idle state configuration */

     TIM1->OISR |= (uint8_t)((uint8_t)( TIM1_OCIdleState & TIM1_OISR_OIS1 ) | 

                 (uint8_t)( TIM1_OCNIdleState & TIM1_OISR_OIS1N ));

      

     /* Set the Pulse value */

     TIM1->CCR1H = (uint8_t)(TIM1_Pulse >> 8);

     TIM1->CCR1L = (uint8_t)(TIM1_Pulse);

    }