Skip to main content
Sameer Damir
Visitor II
Dec 8, 2017 10:26 AM UTC
Question

I need the driver for the EVALKITST8500-1 evaluation kit (Windows 7)

Posted on December 08, 2017 at 11:26

I cant connect to my EVALKITST8500-1 using Smartgrid LabTool V4.4.

The power cable and the USB cable for kit interface are connected properly.

When I connect the interface cable as per the the quick start guide, the LabTool does not recognize any port.

If I go to settings - port: I can find no port to choose

If I go to settings - COM port - Scan port: Again, nothing happens.

In my windows device manager, I can see two new devices which don't have the appropriate driver, there are named: Enhanced COM port, and standard COM port.

#evalkitst8500-1 #smartgrid-labtool
    This topic has been closed for replies.