Skip to main content
LDE S.1
Associate
Sep 1, 2022 12:07 PM UTC
Question

I need hardware error feedback. Or also possible improvements in the design.

I'm using the theseo-liv3f module to make a GNSS board. In this project, I am only acquiring invalid positioning data, and I would like to know if there are any hardware errors to be corrected. I've already paid attention to the reset pin which is actibe low, and making corrections, I managed to update the firmware, but the data is still invalid.

I'm using the active antenna Taoglass AGGBP.SLS.25A

    This topic has been closed for replies.

    3 replies

    AScha.3
    Super User
    Sep 4, 2022 8:53 AM UTC
    • communication with registers/command response is ok ?
    • try as antenna , connect simple piece of wire (ca. 7 cm )
    • C4 10nF , why? i would use 10uF or more
    If you feel a post has answered your question, please click on " Best Answer ".
    LDE S.1
    LDE S.1Author
    Associate
    Sep 5, 2022 8:52 PM UTC

    We use c410nf as decoupling capacitor, because it is the one indicated in the hardware manual for power terminal filtering. Speaking of command response, teseo even sent data to the master, but only invalid data, even managing to update the firmware this problem continued.