Skip to main content
Dzefa.1
Visitor II
May 10, 2021
Question

I'm using RH-PMICL1AK1 which is Engineering model of RHRPMICL1AK01V , its datasheet If the voltage drop on RSENSE exceeds 100 mV, the device enters the current limitation mode.However,actually only the voltage drop on RSENSE exceeds 125 mV.

hello,everyone:

I'm using RH-PMICL1AK1 which is Engineering model of RHRPMICL1AK01V , its datasheet If the voltage drop on RSENSE exceeds 100 mV, the device enters the current limitation mode.However,actually only the voltage drop on RSENSE exceeds 125 mV,the device enters the current limitation mode.Is that the same with you?

blessing.

    This topic has been closed for replies.