Skip to main content
hg-chen
Associate III
May 25, 2007 10:37 AM UTC
Question

Hypertermial received strange data not as expected in baud rate 19200!

Posted on May 25, 2007 at 12:37

Hypertermial received strange data not as expected in baud rate 19200!

This topic has been closed for replies.

4 replies

hg-chen
hg-chenAuthor
Associate III
Apr 23, 2007 9:37 PM UTC
Posted on April 23, 2007 at 23:37

thank you,

It works in UART polling sample code!

in bps 9600 , the hyperterminal responds characters as I typed!

But when I configure as 19200, the hyperterminal responds data not as I typed, for example, I press ''Enter'' 4 times, the hyperterminal responds as 2 question mark ''? ?'' !?

anything wrong?

kaouther
Associate II
Apr 25, 2007 2:06 PM UTC
Posted on April 25, 2007 at 16:06

Could you please precise:

Which product? on which boards? which example used?

thanks.

hg-chen
hg-chenAuthor
Associate III
May 25, 2007 5:27 AM UTC
Posted on May 25, 2007 at 07:27

thank you for reply

basically the clock must be adjust to higher ! then the UART of PC receiving should be OK,

the STR711-SK/IAR tool set and the UART sample code is used ,

the RCCU sample code must also combined with UART sample code

to ensure it works also in high baud rates!

m3allem
Associate
May 25, 2007 10:37 AM UTC
Posted on May 25, 2007 at 12:37

hi kuni,

Do you have always configuration problems with UART communication?

Regards,

M3allem