Skip to main content
saran raj
Associate II
Oct 25, 2017 5:04 AM UTC
Question

How to write option bytes in assembly language for stm8 mcu in stvd

Posted on October 25, 2017 at 07:04

How to write option bytes in assembly language for stm8 mcu in stvd developer using cosmic compiler.

I have to set Read out protection without using the stvp programmer.

    This topic has been closed for replies.

    3 replies

    Thomas G
    Associate II
    Oct 25, 2017 5:55 AM UTC
    Posted on October 25, 2017 at 07:55

    Hi!

    If you translate this bit of Forth into assembly, then here is how to do it.

    Note that '\ ..' and '( .. )' are comments. Data is passed through the data stack, and you can probably keep it in registers when coding it in assembly.

    \ STM8S option setting words

    \ refer to github.com/TG9541/stm8ef/blob/master/LICENSE.md

    \ store char c to (a), inverted value to (a+1)

    : CN! ( c a -- )

      2DUP C! SWAP NOT SWAP 1+ C! ;

    \ unlock write protection, store option byte

    : OPT! ( c a -- )

      FLASH_CR2 DUP C@ $80 OR SWAP CN! \ unlock option bytes

      ULOCK CN! LOCK \ unlock EEPROM, write c to (a) ;

    \\ ULOCK and LOCK from forth.asm:

    ; LOCK ( -- )

    ; Lock EEPROM (STM8S)

       HEADER LOCK 'LOCK'

    LOCK:

       BRES FLASH_IAPSR,#3

       RET

       HEADER ULOCK 'ULOCK'

    ULOCK:

       MOV FLASH_DUKR,#0xAE

       MOV FLASH_DUKR,#0x56

    1$: BTJF FLASH_IAPSR,#3,1$ ; PM0051 4.1 requires polling bit3=1 before writing

       RET

    saran raj
    saran rajAuthor
    Associate II
    Oct 25, 2017 8:32 AM UTC
    Posted on October 25, 2017 at 08:32

    will this work ?

    org 04800h

    LOCKBYTE:dc.b 0AAh; Read out Bytes

    OPT1:dc.b 000h

    NOPT1:dc.b 0ffh

    OPT2:dc.b 081h

    NOPT2:dc.b 07eh

    OPT3:dc.b 000h

    NOPT3:dc.b 0ffh

    OPT4:dc.b 000h

    NOPT4:dc.b 0ffh

    OPT5:dc.b 000h

    NOPT5:dc.b 0ffh

    OPT6:dc.b 000h

    NOPT6:dc.b 0ffh

    OPT7:dc.b 000h

    NOPT7:dc.b 0ffh

    end

    Thomas G
    Associate II
    Oct 25, 2017 5:20 PM UTC
    Posted on October 25, 2017 at 19:20

    No, I don't think that this will work. You can't program the option bytes without unlocking the EEPROM first, and that's something a flash tool won't do while flashing the device.

    You need to solve it either it on the tool chain level (using a programmer like ST-Link), or using IAP (in application programming) with the procedure laid out in

    http://www.st.com/content/ccc/resource/technical/document/programming_manual/0f/82/71/32/87/2a/46/f2/CD00191343.pdf/files/CD00191343.pdf/jcr:content/translations/en.CD00191343.pdf

    Chapter 4.1. That's what the code above does. It's likely that there is also a STM8 library function to do it.