Skip to main content
lzyos
Associate II
Mar 5, 2012 2:59 AM UTC
Question

How to use LSE as clock source of TIM1 or TIM2/3/5 or TIM4

Posted on March 05, 2012 at 03:59

If it's possible to use LSE as the clock source of TIM1 or TIM2/3/5 or TIM4 ?

Use LSE as external trigger of  TIM1 or TIM2/3/5 or TIM4 is accepted too, if possible please share some code sample.

#stm8-timer-lse
This topic has been closed for replies.

2 replies

Nickname13136_O
Visitor II
Mar 13, 2012 12:43 PM UTC
Posted on March 13, 2012 at 13:43

Pls refer example

TIM2_TRIGLSE in

STM8L15x standard peripheral library 1.5.1

Hope this will help.

Reagrds,

konay61
Associate III
Mar 19, 2012 12:57 PM UTC
Posted on March 19, 2012 at 13:57

Hi,

Ive been searching informations about this subject for a while and I found out that LSE isn't able to be used as clock source for TIM1, but is possible for TIM2 and TIM3 as far as I have found so far. As it is said, also there is an example explaining how to do that in STM Library examples..