Skip to main content
ARehm
Associate II
July 29, 2019
Question

How to send command to the NOR flash using SPI?

I'm using STM32L4A6VGx , MT25QL256 NOR Flash connected with SPI. I'm trying to read the ID but didn't get any response except 0.

Here is the code I wrote:

 // Select Pin

 HAL_GPIO_WritePin(Select_GPIO_Port, Select_Pin, GPIO_PIN_SET);

 HAL_Delay(10);

 HAL_GPIO_WritePin(Select_GPIO_Port, Select_Pin, GPIO_PIN_RESET);

 Dev_ID[0] = 0x09E;

 HAL_SPI_Transmit(&hspi2, Dev_ID, 1,10);

 HAL_SPI_Receive(&hspi2, &Dev_ID[1], 1,10);

 HAL_GPIO_WritePin(Select_GPIO_Port, Select_Pin, GPIO_PIN_SET);

//SPI Configuration

static void MX_SPI2_Init(void)

{

 /* USER CODE BEGIN SPI2_Init 0 */

 /* USER CODE END SPI2_Init 0 */

 /* USER CODE BEGIN SPI2_Init 1 */

 /* USER CODE END SPI2_Init 1 */

 /* SPI2 parameter configuration*/

 hspi2.Instance = SPI2;

 hspi2.Init.Mode = SPI_MODE_MASTER;

 hspi2.Init.Direction = SPI_DIRECTION_2LINES;

 hspi2.Init.DataSize = SPI_DATASIZE_8BIT;

 hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;

 hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;

 hspi2.Init.NSS = SPI_NSS_SOFT;

 hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;

 hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;

 hspi2.Init.TIMode = SPI_TIMODE_DISABLE;

 hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

 hspi2.Init.CRCPolynomial = 7;

 hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;

 hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;

 if (HAL_SPI_Init(&hspi2) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN SPI2_Init 2 */

 /* USER CODE END SPI2_Init 2 */

}

This topic has been closed for replies.

1 reply

ARehm
ARehmAuthor
Associate II
July 29, 2019

Its giving either 0 for:  hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;  hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;

giving 225 for:  hspi2.Init.CLKPolarity = SPI_POLARITY_HIGH;  hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;