Skip to main content
ATUND
Associate
May 20, 2019 9:32 AM UTC
Question

How to read the data from M95256 EEPROM?

I'm using M95256 IC which is used as an external EEPROM for the controller. When i'm sending Read Status Register command i can see data from IC in receive buffer. But when i'm sending Read from Memory command, i get only 0xFF data in the buffer.I have checked the Status register after Write to memory command and the WIP = 0 and WEL=1 in the register. I'm not able to see the data on the oscilloscope as well even though i can see Read from memory command is getting transmitted in Tx Buffer as well as i can see it on oscilloscope.

This topic has been closed for replies.

3 replies

Pierre P.
ST Employee
May 20, 2019 10:02 AM UTC

​Hello,

Please follow section 6.5 of datasheet attached.

Warning: Read operation can't be performed if a Write cycle is currently in progress.

Moreover, your status register value should be with WIP & WEL=0. I f WEL= 1 it means the write instruction didn't success.

0xFF correspond to the delivery state.

BR

EEPROM suPPort team

ATUND
ATUNDAuthor
Associate
May 20, 2019 12:17 PM UTC

Hi,

My instructions sequence is:

1.WRITE ENABLE

2.WRITE STATUS REGISTER

3.WRITE DISABLE

4.READ STATUS REGISTER

5.WRITE ENABLE

6.WRITE MEMORY ARRAY

7.WRITE DISABLE

8.READ STATUS REGISTER

9.READ FROM MEMORY ARRAY

I have added delay of 5ms in between the instructions. But still the value of status register remains same i.e. WIP=0 and WEL=1.

ATUND
ATUNDAuthor
Associate
May 20, 2019 12:16 PM UTC

Hi,

My instructions sequence is:

1.WRITE ENABLE

2.WRITE STATUS REGISTER

3.WRITE DISABLE

4.READ STATUS REGISTER

5.WRITE ENABLE

6.WRITE MEMORY ARRAY

7.WRITE DISABLE

8.READ STATUS REGISTER

9.READ FROM MEMORY ARRAY

I have added delay of 5ms in between the instructions. But still the value of status register remains same i.e. WIP=0 and WEL=1.