Skip to main content
itsmejatinus
Associate III
August 1, 2003
Question

How to Read ROM Content?

  • August 1, 2003
  • 4 replies
  • 1103 views
Posted on August 01, 2003 at 09:17

How to Read ROM Content?

This topic has been closed for replies.

4 replies

itsmejatinus
Associate III
July 30, 2003
Posted on July 31, 2003 at 00:57

Does anybody knows, How can i read the ROM Contents? Is it Possible to read it? If yes, Can i also read the option bytes?

sjo
Associate III
August 1, 2003
Posted on August 01, 2003 at 07:07

you can read the rom contents in normal run mode as you would any location in memory. The only way to read the options is IAP mode (if the device supports it) or by external programmer.

Regards

SJO
rolf
Associate II
August 1, 2003
Posted on August 01, 2003 at 07:24

Take care:

if it is realy a ROM device (with metal mask instead of Flash memory) you can NOT read the option byte, neither via IAP nor with an external programmer.

If the ROM device is readout protected, you have also no chance to read the ROM content.

Ciao,

Rolf

shreya
Visitor II
August 1, 2003
Posted on August 01, 2003 at 09:17

Yes it is possible to read the ROM device using STVP7 and EPB. There is a short procedure to be followed. But it is not possible to read the option bytes. For detailed procedure please refer AN1635.