Skip to main content
MAnsa.1
Associate III
February 3, 2021
Question

How to overcome adc fluctuation.

Hiii guys, i am using stm8s003f3.i configure it according to datasheet and it work almost fine,but problem is, it is generating random voltage when there is no input is connected and because of this input fluctuation getting unwanted output.how to make this adc value zero if there are no input connected,please help. here is my ADC initialization and ADC read code.....

void ADC__Initialization (void)
{
 ADC1->CR1_BitFields.ADON = 1; // Turn ON the ADC
 ADC1->CR2_BitFields.ALIGN = 1; // ADC data is right aligned
		ADC1->CR3 |= 0x00; //Disabling buffer
		ADC1->TDRH = 0xFF; // Disable High Schmitt Trigger
 ADC1->TDRL = 0xFF; // Disable Low Schmitt Trigger
}
float ADC__ReadChannel (uint8_t channel)		
{
 uint16_t val;
	 
 
 ADC1->CSR_BitFields.CH = channel; // Select the desired ADC channel
		ADC1->CR1 |= (1<<1); // Continuous conversion Mode.
		ADC1->CR1_BitFields.ADON = 1; // Turn ON the ADC
 do {
 _asm("nop");
 _asm("nop");
 _asm("nop");
 } while (ADC1->CSR_BitFields.EOC == 0); // Wait till conversion has completed
 val = (uint16_t)ADC1->DRH << 8; // Move DRH:DRL into 16-bit return value
 val |= (uint16_t)ADC1->DRL;
 val &= 0x03FF;
 ADC1->CSR_BitFields.EOC = 0; // Clear the end of conversion (EOC) flag
 return (val);
}

Thanks!!!!

    This topic has been closed for replies.

    6 replies

    Uwe Bonnes
    Chief
    February 3, 2021

    Only a voltage source with low enough input impedance can give stable values. A floating input has high input impedance. So pull down the floating input with low enough resistance according to datasheet the and you will read stable values around 0 V

    MAnsa.1
    MAnsa.1Author
    Associate III
    February 3, 2021

    Bro i dont understand what u said,can you please explain in detail how i will get stable 0v at ADC channel???

    Uwe Bonnes
    Chief
    February 3, 2021

    Make a short between the ADC input and ground and test again. If still not stable look for other errors. Datasheet, reference manual ADC section and application notes around ADC can help you.