Skip to main content
cdvehicle
Associate III
Jul 26, 2005 8:54 PM UTC
Question

How to make BIOS default config

Posted on July 26, 2005 at 22:54

How to make BIOS default config

This topic has been closed for replies.

4 replies

cdvehicle
cdvehicleAuthor
Associate III
Jul 5, 2005 1:01 AM UTC
Posted on July 05, 2005 at 03:01

Default the BIOS startup at a splashscreen , it hide the start information such as memory test,PCI device table. I can close

splash screen in BIOS setup, But It is not convenience. How can I

make the default bios config like AMI's config tool?

kaouther
Associate II
Jul 5, 2005 3:41 AM UTC
Posted on July 05, 2005 at 05:41

Are you using an evaluation board? If yes, you should have a jumper to clear the CMOS.

You have also the possibility to reset the setting from the splashscreen in the bios setup.

cdvehicle
cdvehicleAuthor
Associate III
Jul 9, 2005 12:31 PM UTC
Posted on July 09, 2005 at 14:31

Yes, I use the evlboard. I clear the BIOS setup and resetup it. , such as disable spalsh, change Boot disk.....

But ofter few days , when I open the power, the BIOS has changed to default setup. I check the battary, the voltage is OK.3.2V. Why? Perhaps the BIOS is a evalBIOS, so it has some limited?

marios
Associate III
Jul 26, 2005 8:54 PM UTC
Posted on July 26, 2005 at 22:54

If I recall correctly, there is a BIOS menu item that documents what are the different features in the demo BIOS from the regular one. Some timed features.

On the 4.3 version of the BIOS I remember that the board was going in halt mode after a while, with a message sayind ''demo timeout'', preventing the installation of any large operating system.